• Resolved

PCM1755: Zero Detection

Guru 20880 points

Replies: 1

Views: 23

Part Number: PCM1755

Hi,

Does PCM1755 have zero detection function?

As below, it is no description related to PCM1755.

Best Regards,

Kuramochi

  • Kuramochi-san,

    The PCM1755 has the same zero detection functionality as the PCM1753.  The only difference is that zero flag outputs are open-drain on the PCM1755.

    Thanks,

    Paul