but,Some do not change
0x51 00 80 00 00 00 80 00 00 07 80 00 00
0x52 00 80 00 00 00 80 00 00 07 80 00 00
0x27 00 82 01 6c 07 09 a7 2e 00 7b 57 66 00 f6 58 d2 07 82 a7 2e
0x31 00 82 01 6c 07 09 a7 2e 00 7b 57 66 00 f6 58 d2 07 82 a7 2e
0x51 00 80 00 00 00 80 00 00 03 80 00 00
0x52 00 80 00 00 00 80 00 00 03 80 00 00
0x27 00 82 01 6c 03 09 a7 2e 00 7b 57 66 00 f6 58 d2 03 82 a7 2e
0x31 00 82 01 6c 03 09 a7 2e 00 7b 57 66 00 f6 58 d2 03 82 a7 2e
please tell me