Other Parts Discussed in Thread: TPA3255
Hi!
Q1) How should I treat an unused channel? Should the inputs be connected via a small capacitor (e.g. 0.1 uF) to ground? And the outputs connected to BST via a 33 nF capacitor (but NO other connection)?
Q2) When measuring the DC voltage on INPUT_x (pins 5, 6, 16 and 17) of TI eval board I am measuring ~ 6VDC but on my prototype board, I am measuring 3.9 VDC. Is this normal? VDD on my proto is at 12VDC.(and internally generated AVDD and DVDD are fine). Note that the output is centered at PVDD/2 (i.e. 17.5 VDC) as expected but wondering whether this may have an impact on distortion when I will apply an high amplitude signal.
Thank you in advance for your help!
Louis