Other Parts Discussed in Thread: DIR9001, PCM9211
Hi, team,
May I ask the question that is DIR9001-Q1 support TDM? Or only I2S?
Thanks.
Johnny
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, team,
May I ask the question that is DIR9001-Q1 support TDM? Or only I2S?
Thanks.
Johnny
Hi Johnny,
It's not possible to operate the DIR9001-Q1 as an Audio Serial Interface (ASI) bus slave device, which would mean that the SCLK, BCLK, and LRCLK signals would be inputs to the DIR9001, and only DOUT would be an output. The SCLK, BCLK, and LRCLK signals are always outputs with the DIR9001.
However, it is possible to synchronize the SCLK, BCLK, and LRCLK with an external master by feeding in a 5V, 24.576MHz clock as described on Page 16 in the "XTI Clock Source and Oscillation Amplifier" section of the datasheet.
If you look at Figure 7 it shows the clocking tree for the different outputs and that the XTI clock input will directly divide down to drive the SCK/BCK/LRCK outputs which may meet your requirements.
Hi, Collin,
I have one question about DIR9001 EVM.
Below is waveform we tested on EVM through SN74LVU04 to DIR9001 RXIN. Vcc is 3.3V. We tested input signal and pin 1/2/4 signal waveform. My questions:
1. In EVM user guide BOM, R002 is 47ohm, not 47kohm in schematic. Which one is correct for EVM?
2. For SN74LVU04 on EVM, how to design R002 and R003 resistor divider? Inverter output voltage is supposed to be equal to Vcc, but from calculation, pkpk voltage on pin2 is not the same as we tested by scope.
SN74LVU04 schematic in EVM user guide.
CN001 input signal. pkpk is 520mV.
SN74LVU04 pin1 signal, pkpk is 550mV, offset is 1.5V.
SN74LVU04 pin2 signal, pkpk is 2.82V.
SN74LVU04 pin4 signal, pkpk is 3.3V, equal to Vcc.
Thanks,
Johnny
Hello,
I double-checked the BOM that's used to build the EVMs and the R002 component value is supposed to be 47kOhms and R003 is 2.2kOhms which matches the schematic drawing.
There are two things which contribute to the pin 2 behavior
1.) The load is 2.2k which will reduce the VOH/VOL levels due to the increased output current.
2.) When the input to a digital circuit is not a strong logic "0/1" as shown on the Pin 1 voltage, then the output is not driven as strong as it would be if it was.
This is why an additional inverter was added and the Pin 4 output is used for the DIR9001 input.