Hi
I have a TPA3251 configured as mono out PBTL same as datasheet. It was working okay, but failed during testing. (150W mono) no idea why, but it took out one of the PVDD ceramic caps.
I replaced the device and confirmed it is soldered ok however it will now not power up, fault is low. All the input stage/control pins have the correct voltages, GVDD is okay 12V, internal 3V3 regulator is running ok. reset pin functions.
output stage is only 0.7V though. can't see any other issue, so looking for some prompts on fixing where to look