This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

LMK00301: Reliability related questions about LMK00301 and CDCLVC1310

Intellectual 2440 points

Replies: 3

Views: 96

Part Number: LMK00301

Hi team,

When my customer use the LMK00301 and CDCLVC1310, there is a situation that they power off the units but remain input the clock signal in the input pin.

So my customer want to know will this cause reliability problem after using for a long time.

Can you help to evaluate this?

Lacey

Thanks a lot!

  • Hi Lacey,

    It is not recommended to provide a clock input when the devices are powered, this violates the Input Voltage spec given in the Absolute Maximum Ratings Table. Exposure to absolute-maximum-rated conditions for extended periods may affect device reliability.

    Kind regards,
    Lane

    ____________________________________________________________________________________

    To design your own Clock Tree solution, visit WEBENCH Clock Architect ​​​​

    More information Clock and Timing System products: http://www.ti.com/clock-and-timing/overview.html

  • In reply to Lane Boyd:

    Hi Lane,
    Just to double confirm the description.
    The customer said the input clock specs are within the recommended conditions in the datasheet.
    The description you mean in the above post is that the Absolute Maximum Ratings table is just refer to the condition when the unit is powered on.
    If the unit is powered on, we can't not input any signal in the input pin, right?
    Lacey
    Thanks a lot!
  • In reply to Lacey Lin:

    Hi Lacey,

    We suggest to remove the signal on the input pins when VCC is off. Otherwise, there is a risk to damage the device.

    Refer to App notes "ESD Diode Current Specification" to understand it.

    Regards,

    Shawn

    ____________________________________________________________________________________

    To design your own Clock Tree solution, visit WEBENCH Clock Architect ​​​​

    More information Clock and Timing System products: http://www.ti.com/clock-and-timing/overview.html

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.