This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

LMK05318: synchronization of GPS signal

Genius 9585 points

Replies: 2

Views: 117

Part Number: LMK05318

Dear all,

one of my AA is interested to synchronize a 100MHz precise reference with the GPS clock signal (around 2.4GHz).

Since I'm not familiar with this kind of application I was wondering if the LMK05318 can do the job.

regards,

Domenico

  • Hi Domenico,

    Yes, LMK05318 can generate a 100 MHz output clock that is synchronized to GPS-derived reference input, which is typically divided-down to a usable frequency like 10 MHz or even 1 Hz (1 PPS).

    Please see this app note: http://www.ti.com/lit/pdf/snaa324

    We have the LMK05318EVM and TICSPRO GUI software to allow the customer to evaluate this use case.

    Regards,
    Alan

  • In reply to Alan O:

    Hi Alan,
    thanks.
    I'll suggest this part.
    regards,
    Domenico

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.