This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

LMK04828: Minimum LOS Detection Frequency

Intellectual 1730 points

Replies: 1

Views: 85

Part Number: LMK04828

Hello Team,

May I know the minimum LOS detection frequency of CLKin0? 

Customer want to detect LOS of CLKin0 port under this condition. 

CLKin0 : 80kHz, MOS

CLKin_SEL0 : Oputput(push-pull), CLKin0 LOS

Even though customer check that CLKin0 is good and LD1, LD2 are lock, LOS reported as high. It seems like CLKin0 frequency is too low to detect proper LOS detect. 

Best regards,

Alice

  • Hi Alice,

    It is around 370 kHz as datasheet claimed. So the 80 kHz LOS detect is not reliable. Customer need an external method (for example, FPGA counter) to know the 80 kHz status.

    Best Regards,

    Shawn

    ____________________________________________________________________________________

    To design your own Clock Tree solution, visit WEBENCH Clock Architect ​​​​

    More information Clock and Timing System products: http://www.ti.com/clock-and-timing/overview.html

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.