HI I would like to use two LMX2594 to drive two ADCs for interleaving applications. Is there a easy way to configure the LMXs using TICS PRO to have 180 degree phase with each other?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI I would like to use two LMX2594 to drive two ADCs for interleaving applications. Is there a easy way to configure the LMXs using TICS PRO to have 180 degree phase with each other?
Thomas,
As these are differential outputs, it would seem the easiest thing to do is just swap the outputs.
There is no software bit to swap polarity, but you could do this in your layout.
If this doesn't work, you can use the SYNC feature and MASH_SEED bit to program in a delay of 180 degrees as well.
Regards,
Dean