This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

LMK03000CEVAL: USB2ANY firmware loader

Prodigy 10 points

Replies: 1

Views: 216

Part Number: LMK03000CEVAL

  I use USB2ANY connnected to LMK03000C EVM, when connected to PC and open CodeLoader 4, USB2ANY firmware loader window appear, but after I push S1 and Connect USB Connector together, nothing appear. i.e., I can not see the window ready for updating firmware. Could you please help me solve this problem?

  • Homgmei,

    To update firmware, hold the BSL button and plug in the USB. Then stop pushing the button and do the update.

    As TICSPro is much newer, I would try using this with the TICSPro software. It doesn't matter what device you choose as they all use the USB2ANY. Hopefully you have more luck with TICSPro as we are tying to phase out CodeLoader.

    Regards,
    Dean

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.