This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCM6208: use CDCM6208 to generate 15 clocks

Part Number: CDCM6208
Other Parts Discussed in Thread: LMK00304, LMK03328

Hi team,

Can I generate 15 clocks below using 2 CDCM6208?

103.125M, 125M*5, 135M*2 148.5/1.001M, 148.5M, 156.25M*4, 200M

Regards,

Yangbo

  • 148.5/1.001M means the clock is 148.5 divide by 1.001
  • Hi Yangbo,
    Sorry for the delay in response here. You best option would be to use 2, LMK03328's for meeting this requirement (could fall a little short on the total number of clocks required). The first LMK03328 could be used to generate 148. 5MHz, 148.5/1.001 MHz and 135 MHz (x2) using an off the shelf crystal/XO. The second LMK03328 can generate the 4 copies of 156 MHz, 2 copies of 125 MHz, 200 MHz and 103.125 MHz. So you may fall short of 3, 125 MHz clocks that could potentially be addressed via a simple 1: 4 buffer (LMK00304). LMK03328 has superior performance compared to CDCM6208 and has an integrated EEPROM.
    Regards
    Arvind Sridhar