Other Parts Discussed in Thread: LMX2571, LMX2594, LMX2582
Dear colleagues
In my opinion there are several defects in software "TICSPRO-SW" (http://www.ti.com/tool/ticspro-sw at his use with LMX2571:
1. "User Control" tab:
- there are no fields "PLL_N_F1/2" (integer portion of the N-divider).
2. "PLL" tab:
- The field "CP_IDN" is absent. It is possible to make the common field CP_I=CP_IDN=CP_IUP.
- It is impossible to set Fden=2^24=16777216.
- Values of fields don't correspond to values of registers.
- Switching of F1/F2 doesn't update the field "N Divider", "Fden", "FRAC_ORDER", "CDIV", Tx/Rx Power/Ena...
- Prevention at input of N<22 is highlighted at FRAC_ORDER_F1/2 = 3 or 4 - in DataSheet there is no such restriction.
- The fields PFD_DELAY_F1/2 are absent.
3. It is desirable to have the recalibration button = records in R0.
Yours faithfully,
Alexander