The rev E of the datasheet states the following:
A system may transition a device from pin mode to host connected mode by changing the state of the SI_MODE pins and then triggering a device reset (either via the RESETN pin or via setting the RESETN bit in the device registers).
The newest rev G states something different:
A system may transition a device from pin mode to host connected mode by changing the state of the SI_MODE pins and then triggering a device power cycle by toggling the PDN input pin (high-low-high)
Please explain which method is correct or if both methods work and why the datasheet was changed. I am trouble-shooting a system with intermittent problems that followed the procedure in the Rev E datasheet. This system does not provide control of the PDN input; it is a no connect. Given this how can I transition from pin mode to host (SPI) mode ?