My OSC input to the LMK03001 is connected single ended and AC coupled. The datasheet shows the specification for the OSC input is between 0.2Vpp and 1.6Vpp. Does it means that OSC input of 0.2Vpp to LMK03001 will function correctly? The OSC input goes to R Divider and then to the Phase Detector. Can the Phase Detector work correctly with such a low voltage of 0.2Vpp? Is there a voltage range for OSC input for a particular setting. Example : R15(PLL_CP_GAIN[1:0]) ?