Other Parts Discussed in Thread: LMX2492
As per the datasheet of LMX2492, the denominator of the fractional divider is forced to 2^24 when the chip is running the frequency ramping. We are investigating the phase noise at a constant frequency 10.525GHz to begin with (see the graph attached).
1. a fractional of 10485760/16777216, strange phase noise behaviour is observed .
2. a fractional of 5/8, the phase noise seems to be matching the theoretical calculation
Question:
1. Why is there a big difference in the phase noise characteristic when a fractional circuit with the max denominator is used?
2. Is there any difference in setting of the denominator to 2^24 in CW mode and in ramping mode?