This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04610: LMK04610

Part Number: LMK04610
Other Parts Discussed in Thread: LMK04616

Hi,

This is similar to the issue raised earlier. The loop bandwidth for PLL2 is showing to be > 10MHz for a PFD of 10MHz. But this is not observed at higher PFD frequencies.

We need to generate 105MHz and 10.5MHz from LMK04616. for which the the selected VCO frequency is 5880MHz. This synthesis is not possible with higher PFD frequencies. Kindly clarify if the observed loop bandwidth is a tool issue or configuration issue.

The TICSPro file is attached for reference.

Regards,

Ayesha105MHz_10M_PFD.7z