This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

CDCLVD2102: Can CDCLVD2102 accept differential AC or DC coupled CML inputs?

Prodigy 10 points

Replies: 1

Views: 136

Part Number: CDCLVD2102

Hi, 

The CDCLVD2102 datasheet specifies 'universal' inputs can accept LVDS, LVPECL, or LVCMOS. Can the inputs accept DC or AC coupled CML provided the CML driver differential swing and common mode voltage (for DC coupled case) are within the specifications of the CDCLVD2102 differential inputs (spec says it accepts swing 0.3V to 1.6V Pk-Pk and CM of 1 to VCC-0.3)? If so, can you explain if any special certain input network is necessary, and if not can you please explain why not?

Thanks!

  • As long as you do not violate the differential input specifications, it should be fine with the proper input network. Please review the app note below for interfacing considerations. Figures 18 and 19 are of particular interest.
    www.ti.com/.../scaa059c.pdf

    Kind regards,
    Lane

    ____________________________________________________________________________________

    To design your own Clock Tree solution, visit WEBENCH Clock Architect ​​���​

    More information Clock and Timing System products: http://www.ti.com/clock-and-timing/overview.html

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.