This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCUN1208LP: CDCUN1208 - propagation delay - additional info

Genius 11200 points

Replies: 1

Views: 118

Part Number: CDCUN1208LP

Hello Team,

we are currently supporting a new FPGA code that would need to be trimmed to properly interface with the CDCUN1208.

For that design it would be handy to have some additional information for the following parameters.

Table 6.7 - min and Typ. value

Table 6.11- parameter with LVCMOS with 1.8V min and max.

We do not need official min and max value (no need to update the datasheet) but it would help if we have plots or table that include multiple units out of which it could be extracted a max and min value related to the limited number of device under tests.

Thanks,

SunSet

1 Reply

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.