Other Parts Discussed in Thread: CDCLVP1102, LMK61E2
Per the OSC data sheet, the LVPECL Vout, Diff PP is 2xVod = 2x1200mv max= 2.4Vpp. The input of the buffer CDCLVP1102rgtt LVPECL is Vin Diff pp 1.5V max, per it's data sheet. I was planning to connect the two per Figure 19 of the CDCLVP1102 data sheet.
Per the data sheet the OSC output exceeds the input of the Buffer. Am I reading this wrong? It would be odd that both devices being LVPECL can not be connected. How should I connect the two devices? Thank you, Tony