Hello
I want to use LMK04828 in order to achieve two goals:
1. Divide the input signal by 30 and reset the divider at deterministic timing generating a known phase 100MHz clock
2. Generate SYSREF to DAC38RFxx aligned to DACCLK with the proper setup and hold time.
In order to do that:
Fin = 3GHz external input to the part at port Fin, goes to the DACCLK through LMK
One time strobe to sync or sysref input in order to:
1. Reset the divider by 30 to have the clock 100MHz output at a deterministic phase and timing
2. Align the SYSREF to the DACCLK
Can you please advise what is the required setup?
What is the alignment mechanism? Does the LMK moves the SYSREF relative to the DACCLK or the opposite?
Thanks