Hi team,
I see the recommendation for the unused output pin as below:
" For HCSL this would be 50 Ohm to GND. For CML, LVDS, LVPECL you can use 100 Ohm differential termination. For LVCMOS you can just leave the pin open or re-use as a test point with a probing pad."
I have several questions related to the unused output pin:
1. For the unused HCSL, you mean connect both positive and negative pin with 50 ohm to GND.
2. For CML, LVDS,LVPECL, connect the positive and negative pin with 200 Ohm, not need to pull down the pin?
3. For the LVCMOS output, I use the pin mode 8, because it's single end signal, if I just use the positive output(like Y7_P), what should I do to the negative pin(Y7_N)?
Lacey
Thanks so much!