Other Parts Discussed in Thread: LMX2594
Dear Sirs; In using the LMX2592 synthesizer we are trying to control both outputs separately as our application does benefits from both outputs to being used simultaneously. We have many measurements where setting the output level (current from the drives to the load) changes not only the output level (expected) but produces spurious products in the other output. Symptoms include:
1) the effect seems to be output frequency dependent, but not predicable.
2) If we turn off the output not being used the spurious in the desired channel goes away. Not a good option for us.
3) The effect is definitely related to the unused output drive setting, i.e. increasing the drive level makes the spurs higher level.
4) The effect appears asymmetric. The A output suffers much higher spurs with the setting of the driver of the B output than vice versa.
Is there a sequence problem? I expect some crosstalk between the outputs, but this very excessive, sometimes the spurs are as high as the desired signal.