Other Parts Discussed in Thread: USB2ANY
Problem: I have followed instructions from user guide quick start configuration:
1) Connected 4.5V power supply to external jacket
2) 122.88MHz applied to IN1
3) Connected USB2ANY
4) loaded default configuration
ISSUE: The current on the power supply is 0.727A and PLL lock status (STATUS_LD1 and STATUS_LD2) are off
I can manage the PLL lock if not using external VCXO so I suspect problem is coming from there.