Hi Team
I have some questions about LMK03328.
1)Is there any difference in electrical characteristics between crystal input and clean external reference input inputs?
I think that both are the same if you margin the electrical characteristics. Is it right?
2)10.4.3 Crystal Input Interface (SEC_REF)"The programmable capacitors on LMK03328 can be tuned from 14 pF to 24 pF in steps of 14 fF using either an analog voltage on GPIO5 in soft pin mode or through I2C in soft pin or hard pin mode."
I have a question with the above contents.
In Soft pin mode, set with GPIO5. How to set in Hard pin mode?
Best Regards,
Ishiwata