2146.LMK04826B PLL1 LOCKING PROBLEM.pdf
Hi, guys,
I am using PLL1 LMK04826B's CLKIN0 as ref input and OSCin as the external VCO feedback input.
Our PD frequency is 1.536MHz.
We just found out a very odd problem.
Let's say I have a master card that generates ref clock and a slave card that receives the ref clock. the ref clock from the master card is fed into CLKIN0 differential pins of LMK PLL1 of slave card.
we are monitoring the slave card PLL1 R and N divider output on the oscillator scope when PLL1 locks. By keeping the same slave card, but swapping different master cards, we get different relationship between the R divider and N divider output on slave card PLL1, which will be attached during this post.
This is very abnormal since the whole purpose of Phase lock loop is to make R divider and N divider phase relationship constant.
I am aware of that if there is a leaky loop filter capacitor or leaky VCO on PLL1, the phase may not be aligned exactly between R and N divider output, but the phase offset should be constant if I keep the slave card the same。
By the way, We are feeding in a ref clock of 98.304Mhz, it is pulse width modulated ref clock. The pattern is three highs one low and then one high three lows, but the rising edge rate is constant at 98.304Mhz. both the R and N divider is 64, which comes to the PD frequency of 1.536MHz.
Attached you will find pictures of our experiment in the pdf file.
Thank you so much for your help, we have been stuck on this for a couple of days and run out of ideas to try.