I'm currently having a hard time trying to get the LMX 2572 to Ramp. I'd like to set my ramp with the following parameters:
Start Frequency: 100MHz
Stop Frequency: 3GHz
Step: 1MHz
I'm using the TICS Pro software and have read all of the sections dealing with ramping on the LMX 2572EVM Instruction Manual and Datasheet.
I still can't figure out why I can't set the proper values.
Is there a way to quickly test the ramping feature on this board?