Hi,
I hope someone can help me with something confusing that I found in LMK04610 datasheet for the CLKOUTx drive mode and the related options for IBIS file clkout mode.
Datasheet chapter 7.10 describes 4 output options: 4 / 6 / 8 mA HSDS and 16 mA HCSL.
Register map description shows 5 options (e.g. register 0x34 OUTCH1_DRIV_MODE): 4 / 6 / 8 mA HSDS and 8 / 16 mA HCSL (respective settings are 0x10 / 0x14 / 0x18 / 0x3B / 0x3F)
IBIS file shows 7 options:
clkout_cml 1.8V digital Output |16mA HCSL/CML configuration Rload 100ohms
clkout_hsds_8m 1.8V digital Output |8mA HSDS configuation Rload 100ohms
clkout_hsds_6m 1.8V digital Output |6mA HSDS configuation Rload 100ohms
clkout_hsds_4m 1.8V digital Output |4mA HSDS configuation Rload 100ohms
clkout_25_8m 1.8V digital Output |8mA HSDS configuation Rload 25ohms
clkout_25_6m 1.8V digital Output |6mA HSDS configuation Rload 25ohms
clkout_25_4m 1.8V digital Output |4mA HSDS configuation Rload 25ohms
* What does Rload 100ohms or Rload 25ohms in the above IBIS file table actually mean? Shouldn't HSDS always be terminated with 100ohms?
* Can someone please explain which IBIS mode belongs to which OUTCHx_DRIV_MODE setting? clkout_cml is obvious, but how about the others?
* Why is HCSL/CML 8mA setting missing in IBIS options?
* In theory 64 different settings (0x00 - 0x3F) are possible for OUTCHx_DRIV_MODE. Only 6 of them are described in the datasheet. What would be the result if I would use a non-described value? Would that e.g. enable the "Rload 25ohms" option that I can't find elsewhere in the datasheet?
Best regards,
Paul