This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCLVP1216: Fanout of CDCLVP1216

Mastermind 8375 points

Replies: 3

Views: 130

Part Number: CDCLVP1216

Hello,

I would like you to confirm about following configuration is acceptable or not.

* Connect output of CDCLVP1216(LVPECL out) to two LVPECL input device also LVDS input device.

This means fanout number is three (two LVPECL and one LVDS input device.).

My concern is that multiple LVPECL can NOT be connected to CDCLVP1216 due to output current capablity.

(Power supply for CDCLVP1216 is 2.5V.)

However, I'm not sure output current capability of CDCLVP1216, could you please give me your opinion about above configuration ?

Best Regards,

3 Replies

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.