Hi everyone,
I am using LMK04828B PLL in my application for generating three JESD reference clock of 200MHz to FPGA.
These three clock signals are taken from DCLKOUT0, DCLKOUT2 and DCLKOUT12 differential pins.
I have configured these three clock's format as LVDS in internal registers. These Clocks are connected to FPGA through AC coupling capacitor (0.01uF).
While probing I observed the offset voltage of 1.27V in all the three Ouput Clocks at the PLL output pins. While measuring after capacitor(FPGA end), 1.27V offset voltage was removed for the clocks DCLKOUT0, DCLKOUT2 alone. Still Offset voltage of 730mV is observed in the capacitor (FPGA end) of clock DCLKOUT12.
Is any termination circuit needed in receiver end for remove this offset voltage of 730mV?
With Regards,
Santhana Krishnan T L