This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04616: Ref to Out phase variation, alternative device?

Expert 3175 points

Replies: 3

Views: 132

Part Number: LMK04616

Hello,

We have found a major source of phase variation in our system, which is that the "REF-to-out" phase of the PLL that we use to lock to the 250 MHz distributed from the LMK04616 to produce the 6 GHz sampling clock for our RF DAC is not specified, and in fact has a severe (>5 ps/deg C) temperature dependence.

Can you recommend any PLLs that have good REF-to-out phase stability, especially over temperature?

Thanks,
Nick

3 Replies

  • Hello,

    This ticket has been assigned and we'll get back to you soon.

    Regards,

    Hao

  • In reply to Hao Z:

    Hello Hao,

    I wanted to check in on this, any updates?

    Thanks,
    Nick

  • In reply to Nicholas Carley:

    Hi Nick,

    First, are you using the LMK04616 in zero-delay mode? Zero-delay mode routes the output divider back as the feedback, allowing for a much smaller variation in delay between reference and output.

    If zero-delay mode on the LMK04616 is still insufficient to get the desired performance, I recommend using the LMK04832 in zero-delay mode instead.

    Regards,

    Derek Payne

    Texas Instruments

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.