Other Parts Discussed in Thread: LM555
Hello,
I'm using TPL5110-q1, trying to make "60Hz / Pulse width 3.334 ~ 13.336 ms pulse width delay" from "60Hz / pulse width 16.667us input signal".
1. Is this possible to make this work? If they give input signal (60 Hz / pulse width 16.667us) to the “Done pin(Pin number 4), can they have Delayed pulse (60Hz / Pulse width 3.334 ~ 13.336 ms) on the DRV pin(Pin number 5)?
On the “Detailed Description Overview” in the datasheet, minimum timing is 100ms, and this is over than customer spec, which is “pulse width (3.3 ~ 13.3ms)”.
2. There any way to make this reduce from 100ms to around 10ms?
3. Can I make this scenarios with LM555 timer?
4. Those scenarios don’t work, could you recommend proper timer IC that can satisfy this scenario?
Thank you