Good morning everyone.
I should make a project that receives as input the 1PPS signal (+ -30ns jitter) that comes from a GPS.
At the output I have to get a square wave signal of 320Hz, 640Hz, 1280Hz selectable on command (mux).
The txco clock is 10Mhz.
The rising edge of the output signal must be synchronous with the PPS front, but it must be possible to move the phase from zero (in phase) to about 500uSec later than the PPS.
Is it possible to do this using the LMK05318?
What jitter should I expect on the output?
Best regards, Gino