HI,
I need some clarifications of the LMK04828 3-wire SPI interface. I have been trying to look for the standard for this 3-wire SPI. There are many SPI documents in the internet, but most of them are for the 4-wire SPI (SCK, CS, MISO, MOSI). There are some for 3-wire SPI (SCK, MISO, and MOSI) , but they are not the same SPI used in the LMK04828. My questions are:
1. What 3-wire SPI standard this LMK04828 is based on?
2. For a READ on the SPI, is there a requirement for the master to do something on the SCK (such as stretching or delaying the SCK ) at the last bit of address transfer, so there is enough time for the LMK04828 SDIO pin turns around from input to outputting the 8-bit data? And what is SCK delay or turn around timing requirement?
Thanks,
Meng