I am trying to use three LMX2595EVM boards to generate three different synchronized clock outputs (2.4GHz, 3.25GHz and, 4.1GHz). I have tried the methods suggested in documentation without any success. The initial check for synchronization would be getting all three boards generating the same clock and see if they are synchronized, which has been tried without any success. All boards generate the same clock (2.4GHz) without any drift but they are not synchronized. Can anyone please provide some verified solution with a clean connection diagram and links to any TI products necessary to achieve this task?