This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2572EVM: Unpredictable clock drifting.

Part Number: LMX2572EVM
Other Parts Discussed in Thread: LMX2572
We are working with the LMX2572, and we have been having the following issues:
1. When following the simple example given in the instructions (loading the default configuration), we see a peak not at 3GHz, but at about 2.75GHz. 
2. If we change RFoutA to 3200 MHz, we see no change in the output signal. 
3. The PLL lock status LED never illuminates, even after toggling FCAL_EN.
When we power down the unit using User Controls > POWERDOWN, we see the power drop.