This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04208: LMK04208 configuration

Part Number: LMK04208

Hi Team,

One of my customer is using LMK04208 for ZCU111 Xilinx RFSoC. The output Clock frequencies required is as below.

  1. OUT0 -> 7.68 MHz
  2. OUT1 -> 7.68 MHz
  3. OUT2 -> 245.76 MHz
  4. OUT3 -> 491.52 MHz
  5. OUT4 -> 491.52 MHz

 The inputs:

CLKIN0 -> 122.88 MHz

CLKIN1 -> terminated in connector 

Customer requirement is: Feed 10MHz to CLKIN1. Do not use CLKIN0.

Customer have arrived on the values for the configuration they require. Can you please review/validate the attached configuration?

Regards, Shinu Mathew.