Dear TI
I do n’t have LMK04610 EVM or usbany. I designed a board with LMK04610 chip.
I want to generate a set of register values through TICS Pro software and download them to the chip through STM32.
LMK04610 OSCin pin is connected to a 10M high-precision temperature-compensated crystal oscillator
I want to reduce the noise from clkin1, input a 10M, single end clock, use dual loop mode
Output from any of 10 channels to provide a clean 10M clock reference for my other boards
In this case, can you still follow the steps you said, and then download all the registers everywhere to my board's LMK04610 chip to achieve the required functions.
I have another question
I am not quite sure about the status of the board and the status of the configuration program
I want to verify the correctness of my hardware and software by configuring a known pin output of LMK04610
For example: I want to output a high level or the REF clock of the PLL through the STATUS0 pin. I only need to configure 0x009282, 0x009511 (0x00950D), right?
After I used the default configuration, I modified these two registers, but the STATUS0 pin does not change at all, and always outputs a low level.
Looking forward to your reply!
best Regards!
PenJey