This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCLVC1106: Application question

Part Number: CDCLVC1106

Hi,

Customer would like to use our clock buffer for Intel ethernet chip I210, and Intel reference circuit has two cap C1/C2, is that ok to put these cap at our buffer output? Will it impact our buffer performance? 

Regards,

Lynn

  • Hi Lynn,

    47pF load may significantly slow down the edges, and the operating frequency could pose further limitation depending on the edge rate. Could you measure the performance and verify it meets the requirements?  

    Kind regards,
    Lane