Hello,
My goal is to create synchronized low frequency clock (1Hz, 100Hz. 1000kHz) on 2 (or more) different cards, using a 1PPS signal from GPS module at each card
My setup
- LMK05028
- Input 2: 1PPS
- DPLL1: REF-BW 0.008Hz, TCXO-BW 40Hz
- XO 48MHz, OCXO 10MHz +-10ppb
-Output 7: 1Hz, ZDM enable
I want the phase of Output 7 and input 2 is deterministic but I cant achieve that.
Please help meOUT7_1PPS_ZDM.tcs config the LMK05028 to achieve that.
Thanks