This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594: VCO calibration speed:The actual test was 68uS.The manual says it can reach 35uS

Part Number: LMX2594
Other Parts Discussed in Thread: LMX2572

Hi,

When we tested the frequency hopping time of LMX2594 and LMX2572 phase-locked loop chips, the VCO calibration used Partial assist mode, with the output frequency hopping between 1.0g and 1.1g. The frequency hopping time of LMX2594 was 68uS, which could reach 35uS according to the manual.LMX2572 test we found that the actual FM time difference is quite large compared to the manual.

What do we need to improve? Thanks!

  • Hi There,

    Could you provide your LMX2572 configuration? It will be great if you can provide it in TICS Pro format.

  • Dear,

    1875M.txt
    R112	0x700000
    R111	0x6F0000
    R110	0x6E0000
    R109	0x6D0000
    R108	0x6C0000
    R107	0x6B0000
    R106	0x6A0000
    R105	0x690021
    R104	0x680000
    R103	0x670000
    R102	0x663F80
    R101	0x650011
    R100	0x640000
    R99	0x6309E0
    R98	0x621400
    R97	0x610888
    R96	0x600000
    R95	0x5F0000
    R94	0x5E0000
    R93	0x5D0000
    R92	0x5C0000
    R91	0x5B0000
    R90	0x5A0000
    R89	0x590000
    R88	0x580000
    R87	0x570000
    R86	0x560000
    R85	0x55D300
    R84	0x540001
    R83	0x530000
    R82	0x521E00
    R81	0x510000
    R80	0x506666
    R79	0x4F0026
    R78	0x4E0003
    R77	0x4D0000
    R76	0x4C000C
    R75	0x4B0840
    R74	0x4A0000
    R73	0x49003F
    R72	0x480001
    R71	0x470081
    R70	0x46C350
    R69	0x450000
    R68	0x4403E8
    R67	0x430000
    R66	0x4201F4
    R65	0x410000
    R64	0x401388
    R63	0x3F0000
    R62	0x3E0322
    R61	0x3D00A8
    R60	0x3C0000
    R59	0x3B0001
    R58	0x3A8001
    R57	0x390020
    R56	0x380000
    R55	0x370000
    R54	0x360000
    R53	0x350000
    R52	0x340820
    R51	0x330080
    R50	0x320000
    R49	0x314180
    R48	0x300300
    R47	0x2F0300
    R46	0x2E07FC
    R45	0x2DC0DF
    R44	0x2C1FA3
    R43	0x2B0000
    R42	0x2A0000
    R41	0x290000
    R40	0x280000
    R39	0x279680
    R38	0x260098
    R37	0x250304
    R36	0x24004B
    R35	0x230004
    R34	0x220000
    R33	0x211E21
    R32	0x200393
    R31	0x1F43EC
    R30	0x1E318C
    R29	0x1D318C
    R28	0x1C0488
    R27	0x1B0002
    R26	0x1A0DB0
    R25	0x190C2B
    R24	0x18071A
    R23	0x17007C
    R22	0x160001
    R21	0x150401
    R20	0x14E048
    R19	0x1327B7
    R18	0x120064
    R17	0x11012C
    R16	0x100080
    R15	0x0F064F
    R14	0x0E1E70
    R13	0x0D4000
    R12	0x0C5001
    R11	0x0B0028
    R10	0x0A10D8
    R9	0x090604
    R8	0x082000
    R7	0x0740B2
    R6	0x06C802
    R5	0x0500C8
    R4	0x040A43
    R3	0x030642
    R2	0x020500
    R1	0x010808
    R0	0x00241C
    

  • Hi There,

    The setting is for LMX2594 or LMX2572? I think you have issue with LMX2572 only, right?

  • Hi,

    The setting is  LMX2594.

  • so you have problem with LMX2594 or LMX2572?

    I think you have issue with LMX2572, right? if this is the case, would you please provide the LMX2572 setting?

  • Hi ,

    We tested the LMX2594 Demo Board of TI,

    Frequency from 1.8G to 2.5G time is consistent with the manual.The time from 2.5g to 1.8g is longer than the manual.

  • Hi There,

    OK, I think you want to shorten the VCO frequency switching time. Then, what is your target switching time?

  • Hi,

    Partial assist: 35uS

  • Hi There,

    35µs is a very aggressive number, I am afraid it is not always possible with partial assist. You may consider to use full assist, which will bypass calibration and therefore save some switching time. However, you also need to ensure that your loop bandwidth is wide enough to support less than 35µs switching time.

    Please review the following appnote to get a sense of what kind of calibration assist can help you.

    www.ti.com/lit/snaa336