Looking at the requirements for the OSCin pin of the LMK04906, the max single ended voltage is 2.5V. Is there a recommended circuit for driving that input with a standard 3.3V CMOS VCXO?
Looking at the evaluation board, there are two series 0.1uF capacitors that drive the OSCin port. It isn't clear why this would meet the max voltage specification of the LMK when driven by a 3.3V CMOS device.
Also, in the LMK04906 datasheet in figure 39, there is an Rterm resistor shown but no discussion as to what it might be or the input impedance of the OSCin port.
Any guidance would be appreciated.