Hi,
I am using LMX2541SQE2690E in my design. I am planning to generate 1350MHz output with this PLL. My OSCin freq is:80MHz . I am programming this device from FPGA with sclk of 6.5MHz & for LE after loading the each register value kept high for 80ns & then kept low for 80ns.
Both CE & RF_OUT pins are kept high
The following observations are found:
The output frequency observed was 1.35 GHz(if i am not loading the R0)
The output frequency observed was 1.5GHz(after loading all the registers)
The above two frequencys are observed irrespective of my oscin & register values
Clarification:
1. what could be the reason for the output frequency error ?
Kindly help any one to resolve the issue.
Please find the PLL register values which i was used:
R7 0x00000017
R13 0x0000008D
R12 0x0000001C
R9 0x28001409
R8 0x0111CF88
R6 0x001F3316
R5 0xA0000005
R4 0x88002644
R3 0x0D808003
R2 0x04000002
R1 0x00000081
R0 0x000010E0
Regards,
Rajesh