Hello,
We are working on CDCE913 with following configuration:
1. S0 Pin Status: Connected to 1.8V
2. We want to turn ON the PLL
3. Expected O/P Frequency:
Y1 = 0.1MHz
Y2 = 1MHz
Y3 = 10MHz
4. Data Loaded to the CDCE913:
Bit ==> 76543210
Byte 00 - 00000001
Byte 01 - 00000000
Byte 02 - 10110111
Byte 03 - 11101000
Byte 04 - 00000010
Byte 05 - 01010000
Byte 06 - 01000000
Byte 07 - 00000000
Byte 08 - 00000000
Byte 09 - 00000000
Byte 10 - 00000000
Byte 11 - 00000000
Byte 12 - 00000000
Byte 13 - 00000000
Byte 14 - 00000000
Byte 15 - 00000000
Byte 16 - 00000000
Byte 17 - 00000000
Byte 18 - 00000000
Byte 19 - 00000000
Byte 20 - 01101101
Byte 21 - 00000010
Byte 22 - 01100100
Byte 23 - 00001010
Byte 24 - 11111111
Byte 25 - 10100000
Byte 26 - 00000010
Byte 27 - 10000100
Byte 28 - 00000000
Byte 29 - 01000000
Byte 30 - 00000010
Byte 31 - 00001000
Currently we are facing a problem in programming the chip.
We are able to see the Clock and Data pulses on the SCLK and SDA pin but nothing is changing on the O/P, so we are not sure that the data is loaded on to the CDCE913 or not.
The O/P which we are getting currently is the default setting O/P.
Please guide.
Regards,
Richa