Hi Team,
I have a question about CDCE62002 SPI Command Structure.
You can find the SPI Command Structure and SPI Read/Write timing chart in the datasheet, but I cannot understand the bit relation between Figure 15/16 and Figure 17.
[Question 1]
What is the bitX relation between Data Field bits in Figure 17 and Figure15/16 ?
Please confirm if my recognition is correct.
<Figure 17> <Figure 15 or 16>
Data Field bit27 = bit0
Data Field bit26 = bit1
Data Field bit25 = bit2
...
Data Field bit1 = bit26
Data Field bit0 = bit27
[Question 2]
What is the bitX relation between Figure17 Addr Field and Figure15/16 ?
Please confirm if my recognition is correct.
<Figure 17> <Figure 15 or 16>
Addr Field bit3 = bit24
Addr Field bit2 = bit25
Addr Field bit1 = bit26
Addr Field bit0 = bit27
Best Regards,
Kawai