Hello,
I recently had a post on this forum about this chip, and Patrick was a huge help:
http://e2e.ti.com/support/clocks/f/48/p/357511/1260454.aspx#1260454
I'm using a DAC34H84 EVM, which has a CDCE62005 clock chip on it. I'm using this clock for the FPGA on a TSW1400, and am troubleshooting some bad looking outputs on the DAC. What I'm currently trying to do, is use an external reference into the CDCE62005, rather than using the onboard 19.2 MHz crystal.
My problem is- I can't get the crystal to disable. Using the DAC GUI, I have the Primary input enabled with a divider of /1, and the secondary input is tri-stated. However, for some reason, the Secondary (crystal) signal is still be fed to the VCO. I am measuring output three, which goes to my FPGA.
My settings are:
Input Divider = 48
Feedback Divider = 500
Bypass Divider = 5
Y3: Source = VCO, Enabled, Divider = 16
For a 19.2 MHz secondary, I expect:
19.2 MHz * 500 * 5 / 48 / 16 = 62.5 MHz
This is exactly what I get. Note- this is with the secondary tri-stated, and the input source set to Primary in! I don't even have an external clock connected. When I do, I am using a 15 MHz from 0V to 1.3V (is this incorrect?). I have my configuration file attached.
Thank you,
Nicholai