This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCVF25081 16pin connection

Other Parts Discussed in Thread: CDCVF25081

Hi,

I would like to ask you 2 questions about CDCVF25081 16pin connection.

Q1) Must 16pin be connected one of 8 outputs (1Y0 - 1Y3, 2Y0 - 2Y3)?

       If yes, for example, 1Y3(15pin) is very useful to connect due to next pin, I think.

       What do you think of 15pin connect?

Q2) Is it necessary to use "capacitor" (for example, 10pF) between 16pin and GND to prevent signal overshoot/undershoot from occuurring?

Thank you very much in advance for your support!

Best Regards,