Hi
LMX2581
Input 150MHz clock from RFin, Can you output the 150MHz to RFoutA as it is? (RFin 150MHz ⇒ RFoutA 150MHz)
following register setting OUTA_MUX : "2" MODE[1:0]: "1" (PLL Only Mode)
I am aware that the specifications of RFin is 0.5 ~ 2.2GHz.
I think that is only through to RFout from RFin, and not affect the frequency limit of 0.5GHz, but how might it be?
Best regards