I am seeing that the TOF2 and TOF3 frame rates are cut in half when I use auto align. For example, when programming PLL3 fro 23.98 Hz output, with reg 0x13 set to 0x00, I get 12 Hz TOF3 rate. If I program reg 0x13 to 0x20 i get the proper 23.98. Is this a known issue? I thought i read elsewhere on here that Always Align could lead to increased jitter.
TIA Dave