I'm using a CDCLVP1204 clock driver at 360MHz, and when I look at the output phase between OUTPx and OUTNx, I see very little phase shift (maybe 10 degrees). As I change my clock frequency, the phase between the output changes. At 270MHz, they are beautifully 180 degrees out of phase, at 110MHz, they are back to being close to in phase.
The actual application for this has the outputs pulled to ground through 150 ohm resistors, and at the receiver end (a DAC5682z), they are capacitively (.01uF) coupled to a 100 ohm differential terminator. I tried disconnecting the terminating end (lifted the two caps), but this didn't seem to have much of an effect.
What could be causing this performance? This device is supposed to be capable of operating up to 2GHz.
Thanks,
Barry