Hi,
We are planning to use ADC12D1800 in my application. In my board there will be two devices(12bit ADC from TI & front end Track & hold HMC661LC4B amplifer from Hittite) which requires same clock of 3.1GHz. I planned to use LMX2541 PLL for clocking the ADC as well as track hold amplifer but LMX2541 has single channel o/p for this I planned to use LMK01801 has a clock distributor between PLL & ADC whether this will work ?
What will be the performance degradation due to LMK01801 in the chain?
Is there any other device which is better than LMK01801 ?
Whether LMX2541 shall drive LMK01801 directly ?
Note: My board has two independent analog channels, Two adc channels two PLL chips both the channels are operating at different sampling frequency's. So I planed to use both the channels in the LMK01801 chip .
Regards,
Rajesh